1/5/2021 1:43 PM | |
Joined: 9/30/2016 Last visit: 8/13/2025 Posts: 946 Rating:
|
Please also see the attached screenshots. I have just installed Startdrive Advanced V15.1 UPD3 on our PG and (which is not allowed to be connected to the internet). I also downloaded the Startdrive_V15_1_HSP_FW_V4_7_SP13.zip file so I could update the HW and FW. The installation of Startdrive went without problems but I cannot install the updates. When I try (from inside the TIA portal it say I have to close the TIA Portal and that the update will start after I close the TIA Portal. But it does not start. What am I doing wrong and how do I get the updates installed? AttachmentSD Updates A.zip (396 Downloads) |
Follow us on