6/17/2024 9:03 AM | |
Joined: 6/16/2023 Last visit: 10/29/2024 Posts: 1 Rating: (0) |
Hello, If I have a project in PCS 7, and I want to insert alarms that are on an S7-300 connected via TCPIP, will this not interfere with the alarms in the rest of the project? I have the Alarm tags in Tag Management and in the Symbol Table. In Alarm Logging do I have to create a new Message Type? Does this have any restrictions regarding the name? Regards, ___________________ Filipe_M ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 06/17/2024 10:52:06New subject after splitting |
|
Follow us on