12/16/2019 5:47 PM | |
Joined: 9/13/2019 Last visit: 8/23/2025 Posts: 44 Rating:
|
Hello , I would like to ask for help as im begginer with sinamics starter , im using -- G120 PM 240 , CU 240E-2DP and probably newest firmware ,, im connected directly through usb without profibus or profinet and master device.Just have push buttons for simulating . I have 3 NO pushbuttons(Connected to DI1,DI2,DI4) , one pushbutton im trying to use for start the motor with some fixed speed , and another pushbuttons im trying to use for simulating limit switch . I want for my application to work it like this - i start motor with one pushbutton and then when motor reaches the limit motor stop , need to work on both directions , and then i need another application which will start the motor, then motor will stop after reaching the limit and after stopping motor will go to other direction where motor again after reaching limit will stop and repeat. I never tried something like that i don´t know how exact should i set up thins and assign parameters,i have found limit parameter and found also similar issue like mine but still didn´t figure out how should it work properly. So if anybody would have some spare time please show me some screens how should i assign the parameter to work it fine . Here are some screens from my program of what i have tried. AttachmentScreens.zip (314 Downloads) |
Follow us on