1/21/2025 4:49 PM | |
Joined: 9/14/2023 Last visit: 4/6/2025 Posts: 7 Rating:
|
Were you able to solve the problem, would you mind sharing the solution for that??? I guess I am facing the same problem as yours. Actually we have two Siemens FM MAG 6000 devices, each of them is connected to one PTP module. Tx and Rx indicators seem to be blinking in one of the module, but when I looked at the Modbus RTU section and further "Frame Status" in the device, the numbers of Parity and Frame errors are increasing. But I specified the type of parity, stop bits and etc. correctly. And only Tx indicator is blinking in another PTP module meaning request is sent but there is no answer from the deivce, right? What can be done? What am I missing? ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 01/21/2025 19:25:29New subject after splitting |
|
Follow us on