3/13/2008 9:39 PM | |
Joined: 4/6/2006 Last visit: 6/24/2025 Posts: 604 Rating:
|
Hi Patrik, A lot of information about the ET200S and the maximum of the station can be found with the following link. On the site is also a download available on the ET200S configuration tool which helps to create an ET200S without Step 7. And additionally it's also possible to export the data from the tool to import it in Step 7. ET200 Page |
Best regards, |
|
Follow us on