6/19/2025 11:24 AM | |
Joined: 6/19/2025 Last visit: 6/19/2025 Posts: 1 Rating:
|
I want to know how to download micromaster 440 GSD file to connect the VFD with QJ71pb92d module |
6/20/2025 10:45 AM | |
Joined: 9/21/2012 Last visit: 9/16/2025 Posts: 4711 Rating:
|
MICROMASTER 411, 420, 430 und 440: Amended PROFIBUS GSD files |
Last edited by: Moderator_Lan at: 06/20/2025 11:36:57link optimized |
|
6/20/2025 12:42 PM | |
Joined: 9/27/2006 Last visit: 9/16/2025 Posts: 12409 Rating:
|
Hello Ustaad; If you open the zip file inside Hati's link, to look at the MM4 gsd file, you will see that the gsd file is operatiopnal only if you have installed a MM4 Profibus optinal board, 6SE6400-1PB00-0AA0, on the drive. Do you have access to this module on your Siemens drive? They are now considered a spare part, difficult to find in the market. If you do have one, look at the following link, and download the Operating Instructions manual for this module, to understand hopw to use it as a Profibus slave, essentially to manipulate the oindividual bits in the Control Word (for start/stop of the moptor), and the speed Reference word to set the rotational speed on your motor's shaft. Come back to the forum if you need more information. https://www.industry-mobile-support.siemens-info.com/en/article/6SE6400-1PB00-0AA0/man Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 06/21/2025 11:05:20 |
|
This contribution was helpful to
1 thankful Users |
Follow us on