3/27/2025 9:22 AM | |
Joined: 12/20/2023 Last visit: 6/5/2025 Posts: 6 Rating:
|
Hi, I found this post: Missing PG/PC interfaces on Windows 10 - 210351 - Industry Support Siemens tried to solve issue on my PG but it didn't work. Missing interfaces, anytime I start working with TIA (v16 mostly) the interfaces are missing, only TeleSync stays in the list. So far only temporary solution for me is to run (admin) the "s7oiehsx64.exe" file. Then my interfaces are coming back to life. The reason of why it\s missing I'm not sure, but it might got something to do with using "CCLeaner" with deep analysis and cleaning also some broken registry keys. But as I wrote, I'm not sure of it. No update of Windows, or TIA in that time happen, so it's not that. I tried to find the missing registry key, but it is different then described above; it is few years later, so perhaps it changed as well. If anyone could help me with it, I apprecciate really. Added one line (marked in yellow on attachement) - please correct me if it's wrong. I search the "path" within "siemens" folders in registry to find it. kind regards Mariusz ------------------------------------------------------------------------------------------ |
Last edited by: mariusz_kiczka at: 03/27/2025 09:24:27Last edited by: Moderator_Lan at: 03/27/2025 10:15:35New subject after splitting Last edited by: mariusz_kiczka at: 03/27/2025 16:35:53 |
|
Follow us on