3/8/2019 5:23 PM | |
Posts: 7 Rating: (2) |
May I suggest for anyone needing 24Vdc I/O's to have a look at this board https://www.st.com/en/ecosystems/x-nucleo-plc01a1.html It makes for a great 24Vdc 8x IN + 8x OUT for a standard Arduino but as far as I know it has no libraries so one would need to program it the old fashion way by reading the chip specifications and writing code for it! And only fits the IOT when the upper half plastic case is removed! Dam... |
This contribution was helpful to1 thankful Users |
7/2/2019 12:44 AM | |
Joined: 4/28/2015 Last visit: 8/9/2019 Posts: 10 Rating: (0) |
In other worlds you need a driver for using it? |
2/5/2020 10:12 AM | |
Posts: 15 Rating: (1) |
Are these shields suitable for all variants of the IOT2000? I have a Mindconnect IOT2040. Do the shields fit there too? |
3/19/2021 9:38 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (171) |
New question published by anasnadakkavil is split to a separate thread with the subject Arduino Shields for iot2050. Best regards |
Follow us on