9/28/2023 6:07 PM | |
Joined: 11/11/2022 Last visit: 7/11/2024 Posts: 7 Rating: (0) |
After experimenting some more today, I do have another issue that I want to eliminate but have difficulty with. The burner can still burn prolonged when the living room thermostat asks to burns 39 min but when the water thermostat could start it would add another 20 min. That's something I am trying to avoid. The total burn time is too close together (39min + 20min). The problem is that the timers reset immediately in case the thermostat goes low. I need the behaviour of a retentive On-Delay that it counts independent from the thermostat lows, but the output remains high. Is there a solution to this? I have been trying but could use some help. ------------------------------------------------------------------------------------------ |
Last edited by: AutoGen_8133711 at: 09/28/2023 18:11:53Last edited by: Jen_Moderator at: 09/29/2023 08:32:32New subject after splitting |
|
9/28/2023 6:44 PM | |
Joined: 11/11/2022 Last visit: 7/11/2024 Posts: 7 Rating: (0) |
If they can be added together that would be the safest way. |
9/28/2023 6:59 PM | |
Joined: 11/11/2022 Last visit: 7/11/2024 Posts: 7 Rating: (0) |
I couldn't have written it in a better way. I keep hitting the problem of not finding the right pulse timer in logo. |
9/28/2023 7:50 PM | |
Joined: 12/18/2014 Last visit: 10/14/2024 Posts: 33954 Rating: (4221)
|
Try this.
AttachmentBurner_0BA8.Standard.zip (549 Downloads) |
This contribution was helpful to1 thankful Users |
9/29/2023 9:03 PM | |
Joined: 11/11/2022 Last visit: 7/11/2024 Posts: 7 Rating: (0) |
I definitely couldn't have come up with that myself but seeing that diagram it does make total sense. About the long breaks, I added a 25 min reset to the stopwatch in case the burner has not been active. That's some fine designing ixo, respect to you, I learned a lot from that diagram. Here is how I modified it to reset after 25 min of inactivity on the burner. I hope I did a good job, this is exactly how I want it. (the diagram is in seconds for simulation). Attachment2 Thermostats prolonged burner prevention + inactivity reset.zip (496 Downloads) |
Follow us on