4/26/2025 8:52 PM | |
Joined: 9/6/2023 Last visit: 8/27/2025 Posts: 6 Rating:
|
Hi, you can configure baudrate with jumpers 1 and 2, maybe this file can help you until you get the configuration tool.
AttachmentUH50-RS485B-mont-v1.5-en.pdf (445 Downloads) |
This contribution was helpful to
2 thankful Users |
5/19/2025 11:00 AM | |
Joined: 5/30/2014 Last visit: 9/15/2025 Posts: 173 Rating:
|
Hi, This is a very old version of this module, powered by 12 (8-24) VDC. Newer version WZU-485E-MOD works with 24 VAC and they cannot be interchanged and configured without the software (the datasheet is attached). There was strange response from the L&G: they sent me credentials for the access, but it hadn't enough privileges to download. After my complain, they never responded. However, I tried that later again and it worked?!?! The software (v1.45) is also attached. P.S. I really don't understand relationship between Siemens & L&G, selling partially hardware and software for its configuration. AttachmentWZU485ConfigurationTool and datasheet.zip (302 Downloads) |
Last edited by: C-3PO at: 05/19/2025 11:04:52If you find my contribution helpful please RATE it :)) |
|
Follow us on