5/23/2024 12:56 PM | |
Joined: 2/1/2010 Last visit: 9/27/2024 Posts: 150 Rating: (71) |
Is it all instances of the interlock block faceplate or just that one protect only? Did you modify the faceplate files? When you said you ran OS project editor and make new client, do you mean from OS project editor of your OC or the physical machine? Maybe your @PG pdl for the faceplate in the client project is corrupted, try to copy it from the OS project or rerun OS project editor on the client project and redownload. |
If my post helped you, please rate. Thanks. |
|
5/23/2024 6:07 PM | |
Joined: 2/1/2010 Last visit: 9/27/2024 Posts: 150 Rating: (71) |
What's the quality code of the affected variables (OSPerm, .OpSt_Out, etc)? Seems like a quality code animation issue being gray like that. But that doesn't explain behavior difference between client and server unless your PG pdl files aren't the same. Copy all the @PG files for related faceplates types (Intlk2/4/8/16) from the OS server project GraCS on the ES (working correctly per you) to the OC project GraCS on the ES (not working correctly) and redownload the client. - This rules out corrupted @PG files in your client project(s). Do the same for scripts if you really think your scripts are corrupt on the OC, but scripts have nothing to do with all those tags not linking per your screenshot. The bottom half of the page does rely on scripts but that part isn't having an issue. If that doesn't work - reinstall the client PCS7 from blank windows and redownload the client project. - Ensures restore factory scripts. If that doesn't work then you likely need to escalate to Siemens via SR. |
If my post helped you, please rate. Thanks. |
|
5/24/2024 12:27 PM | |
Joined: 2/1/2010 Last visit: 9/27/2024 Posts: 150 Rating: (71) |
You switch back to the "standard" faceplate and it still not working, or just the "preview" page? I took it as only the preview page was broken based on your initial description and screenshots. |
If my post helped you, please rate. Thanks. |
|
Follow us on