1/16/2023 3:28 PM | |
Joined: 9/29/2019 Last visit: 9/17/2023 Posts: 1 Rating:
|
Dears , I want control 16 servo Axis ( independent) for position control ( V90 or S210) with S71500T PLC. could you suggest which Technology PLC can be used to control the position for 16 Axis? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/17/2023 09:08:20New subject after splitting |
|
1/17/2023 9:19 AM | |
Joined: 1/21/2013 Last visit: 7/22/2024 Posts: 3005 Rating:
|
Hi danizzz, you can use the TIA Selection Tool to select the right PLC. It can calculate the CPU utilization according to your requirements. For a motion control cycle of 4ms the tool recommends technology CPUs beginning from CPU 1516T-3 PN/DP or the CPU1515SP PC2. Kind regards |
This contribution was helpful to
1 thankful Users |
1/17/2023 9:19 AM | |
Joined: 12/23/2021 Last visit: 2/21/2024 Posts: 234 Rating:
|
Hi! The number of axes affects the cycle time of the PLC program. You can use TIA Selection Tool to check which CPU can best suit your specific needs. In the following link you can also see more information about standart application controls with S7-1500/T CPUs. SIMATIC S7-1500 / S7-1500T: Standard application axis control |
If this post helped you in any way, please rate it positively. |
|
This contribution was helpful to
1 thankful Users |
Follow us on