10/17/2010 5:47 PM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Hello, Look at Wincc V WinCC flexible. Perhaps you could use virtual machine. In one will use Flex in the other WinCC. Even is possible to install them together. (depends of their versions). best regards, Hristo Mihalev |
10/18/2010 1:50 AM | |
Joined: 10/7/2005 Last visit: 9/14/2025 Posts: 3049 Rating:
|
Hello fury_omen as UMENCHO said, you can have WinCC and WinCC flexible installed together if that's what you are after and below are two links concerningversioncompatible(note also the additional links at the top of each page): Which SIMATIC software components are released for SIMATIC WinCC flexible 2008? With what are SIMATIC WinCC V7.x, V6.x and V5.x compatible? WinCC flexible and WinCCdiffer considerably from each other engineering wise though and you won't be able to convert our flex application to a WinCC application. I hope this helps |
Cheers |
|
Follow us on