7/11/2025 8:44 AM | |
Joined: 8/3/2009 Last visit: 9/9/2025 Posts: 16368 Rating:
|
Hello Thomas_Drst The Unified Configuration dialog takes a bit of time to run till the end, I would say 1-2 minutes. You should check if you have set up everything correctly: https://support.industry.siemens.com/cs/de/de/view/109806850 Also you should check if you use the latest Update for your TIA Portal (Upd3) and the Unified PC RT (Upd2). Check also if you Windows User does have administrative rights and is member of the Siemens TIA Engineer and the local Siemens user groups. Bye Murof |
If this Information really helps, you could use the Rate function |
|
7/11/2025 10:57 AM | |
Joined: 5/30/2024 Last visit: 8/13/2025 Posts: 7 Rating:
|
Thank you for your reply Murof. I've managed to make a bit more progress — I can now load a page when I enter the PC’s address, but it displays an error (attachment). From what I’ve seen, it might be related to some IIS features not being enabled. I followed this configuration guide to activate the various features : https://support.industry.siemens.com/cs/mdm/109773078?c=128052276619&lc=en-FR I'm not sure if there are other features that need to be enabled specifically for Unified. I tried running the Station Configurator several times (by the way, the web configuration takes at least 30 minutes on my machine). I also saw here:https://sieportal.siemens.com/en-fr/support/forum/posts/wincc-unified-iis-error-500-1013/243820 that someone managed to fix the error by reinstalling Windows. I might give that a try... Thomas |
Follow us on