6/14/2024 11:05 AM | |
Joined: 2/25/2016 Last visit: 7/22/2024 Posts: 7 Rating: (2) |
Good afternoon, has anyone tried making a CustomWebControl to display 3D files with ThreeJS library. I am doing experiments and have had some success on WinCC Runtime (Windows). But here is a question whether the same component will work on HMI panel? Such as MTP700 for example. Can anyone test these two components, one checks if WebGL technology is supported on the panel and the second one should actually display 3D object (Hourse). AttachmentCustomWebControl.zip (67 Downloads) |
6/20/2024 9:00 AM | |
Joined: 8/21/2014 Last visit: 8/16/2024 Posts: 1006 Rating: (13) |
Closed cause question posted twice. The second thread with the subject 3D CustomWebControl for HMI Unified Panel is published within the conference WinCC Unified Systems Best regards, |
My Forum is the place to personalize your profile, |
|
Follow us on