2/16/2022 7:47 AM | |
Joined: 5/20/2019 Last visit: 10/21/2024 Posts: 4 Rating: (0) |
Dear Sir Please let me know as question below 1. Is it possible Sitans SL for O2 with range 0 - 25% can change on site by user becomes 0 - 100% Volume. If Possible please let me know how to change . 2. Our customer have data as below Pressure 1013 mbar Path Lenght .0.5 meter Temperature 0 - 400 Deg F N2 63.65% NO2 70 mg/Nm3 SO2 10 mg/Nm3 C3H8 25 PPM CO 37500 mg/Nm3 Ar 0.87% CO2 8% H20 9.46% O2 18% they need to install the LDS6 for CO, CO2 beside the CEMS cabinet, not on Stack. Please advice whether the LDS6 can work properly . BR ------------------------------------------------------------------------------------------ |
Last edited by: AutoGen_7336015 at: 02/16/2022 07:49:11Last edited by: Jen_Moderator at: 02/16/2022 11:43:28New subject after splitting |
|
Follow us on