10/11/2022 6:51 AM | |
Joined: 5/6/2022 Last visit: 9/27/2024 Posts: 455 Rating: (90) |
Hi AutoGen_405089! Adding to what sancruz said, I would simply add that a downgrade of the equipment can also irreparably damage the CPU, so it would be better to look for an alternative solution. Best regards! |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to2 thankful Users |
10/13/2022 3:52 AM | |
Joined: 3/25/2013 Last visit: 2/21/2024 Posts: 3 Rating: (0) |
CPU 1215FC DC/DC/DC (6ES7 215-1AF40-0XB0) Hardware version FS14 Firmware v4.5.1 Thank you |
10/13/2022 6:24 AM | |
Joined: 1/21/2013 Last visit: 9/28/2024 Posts: 3140 Rating: (489) |
Hi, the FS14 is the latest functional state, it should support all current available firmware versions starting at V4.2. Since I at the moment count 3 similar questions, I would recommend you to contact the technical support creating a new support request. Kind regards
|
This contribution was helpful to1 thankful Users |
Follow us on