1/14/2022 3:49 AM | |
Joined: 10/22/2018 Last visit: 8/8/2024 Posts: 4 Rating: (0) |
HI Dawn thanks for your reply my issue is the Ultramat 23 values to PLC ( 4-20mA ) hardwired drops to zero after like 20 min. this happens when the module is switched on. i suspect the motherboard has an issue now i am thinking of another option where I can communicate the measured values to PLC. I do not have optional profibus card installed. only an serial Port Kinyanjui ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/14/2022 11:43:06New subject after splitting |
|
1/14/2022 11:46 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice. The second thread with the subject ULTRAMAT 23 Measuring Problem: 0 values are displayed at the outputs on the DCS is published within the conference Process Instrumentation / MI Digital Solution / Valve Positioner / Analyzer Systems / Continuous and static Weighing Technology . Best regards, |
Follow us on