1/16/2020 10:06 AM | |
Joined: 11/16/2018 Last visit: 3/6/2022 Posts: 1 Rating:
|
你好,为什么我的wincc Unified无法与1200通讯,wincc Unified屏幕上的变量无法从PLC中得到。 h ello,warum kann mein WinCC Unified Nic mit 1200 kommunizieren?Die Variablen aufdemWinCC-Unified-BildschirmkönnennichtvonPLC bezogen werden [Please use english in the english forum: Hello, why can't my WinCC Unified not communicate with 1200? The variables on the WinCC Unified screen can't be referenced by PLC] ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 01/16/2020 17:35:17New subject after splitting & Added English |
|
1/19/2020 2:27 AM | |
Joined: 2/9/2015 Last visit: 5/9/2024 Posts: 11 Rating:
|
PC/PG接口没有设置正确,在控制面板里面需要设置的。 Configure PC/PG Interface. |
6/5/2021 11:23 AM | |
Joined: 9/23/2005 Last visit: 8/13/2024 Posts: 4347 Rating:
|
Hi, As form TIA V17 it is possible to use PLCSIM together with WinCC Unified. This makes it possible to test systems simulating both PLC and HMI communicating with each other. It also make possible to simulate project with s7-1200. SIMATIC STEP 7 incl. Safety, S7-PLCSIM and WinCC V17 TRIAL Download |
Denilson Pegaia |
|
This contribution was helpful to
1 thankful Users |
Follow us on