10/21/2020 8:36 PM | |
Joined: 10/3/2017 Last visit: 9/12/2024 Posts: 4 Rating: (0) |
Hi all, Is their any official open-source library available from Siemens regarding S7 communication to use directly in projects instead of using node-red? As an example; we are currently using snap7 in a Qt application to import the necessary library. However, I'm looking towards a more official way of doing things as this project has not been maintained for quite some while. Regards, |
10/22/2020 10:50 AM | |
Posts: 22 Rating: (0) |
May be... you could try this: http://settimino.sourceforge.net/ |
10/22/2020 3:24 PM | |
Joined: 10/3/2017 Last visit: 9/12/2024 Posts: 4 Rating: (0) |
@Bergmanu, does Siemens provide any closed source library for Linux? |
10/23/2020 5:20 PM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating: (60)
|
Hello, You can find the s7classic protocol as open source library but not s7plus. S7plus is also not available as a standalone library for Linux, but we have them running on different products in our potfolio such as Edge Devices and the Siemens App "S7-Connector". Kind regards! |
11/25/2020 9:22 AM | |
Joined: 4/28/2015 Last visit: 9/9/2024 Posts: 3345 Rating: (379)
|
Hi, you can use these 3rd party open source libraries for PLCs 300/400/1200/1500 and the LOGO! as well. There is snap7 and also node-s7 (which is also the base for the s7 node-red node). Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on