5/23/2024 7:39 AM | |
Joined: 9/27/2017 Last visit: 5/23/2024 Posts: 1 Rating: (0) |
Good Morning, A customer want add a OPC UA Communication to a CPU 1513 installed on 2019 with Firmware 2.5(6ES7 513-1AL02-0AB0) and TIA V15. I'm going to make an offer for to do this job. Can someone tell me if I upgrade the firmware of the CPU to 3.0 and I buy a CP 1543-1 and upgrade the project to TIA V 17, then the OPC communication will work on CP Port? I don't want to use the CPU port for safety reasons. Thank you. Riccardo. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/23/2024 09:10:45New subject after splitting |
|
5/23/2024 9:19 AM | |
Joined: 3/11/2019 Last visit: 6/17/2024 Posts: 1477 Rating: (266)
|
Hi, as mentioned in the original post, yes it will. The preconditions are met after firmware upgrade of the CPU and the usage of a TIA version this firmware can be configured. Hint: Information can also be found here: How can an OPC UA access to the SIMATIC controllers S7-300, S7-400, S7-1200 and S7-1500 be established?**EDIT** Please also check the firmware of the CP itself! There are also preconditions, stated in the known posts. regards sancruz |
Last edited by: sancruz at: 05/23/2024 09:28:55Feedback appreciated, please rate |
|
Follow us on