5/23/2024 6:09 AM | |
Joined: 5/22/2012 Last visit: 5/23/2024 Posts: 3 Rating: (0) |
HI Is it possible to connect and send data with the 400 Ridandnet system in Modbus TCP, IP mode? Thank you ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/23/2024 08:47:34New subject after splitting |
|
5/23/2024 6:13 AM | |
Joined: 5/22/2012 Last visit: 5/23/2024 Posts: 3 Rating: (0) |
hi I have the same problem I want to do the same thing If your problem is solved, please send it to me Thank you
|
5/23/2024 10:10 AM | |
Joined: 3/11/2019 Last visit: 6/17/2024 Posts: 1477 Rating: (266)
|
Hi, in general there are librarys and also licenses available for CPU-400 and redundancy. So yes, it should be possible. And there are a lot of FAQs and application examples from Siemens available. Just a few: Which technical data applies for the SIMATIC Modbus/TCP blocks and for which CPUs and CPs is it released?-> Redundancy How many devices can you connect to an S7-300/S7-400 using the Modbus/TCP protocol?-> Redundant communication Modbus/TCP - Standardized and redundant Communication of PCS 7 with Third-Party SystemsBlock library for redundant Modbus/TCP communication via CP443-1 or CP343-1regards sancruz |
Feedback appreciated, please rate |
|
Follow us on