2/3/2020 9:08 AM | |
Posts: 1 Rating: (0) |
Hi, I am new to programming so please excuse if this is silly, I am trying to program profibus slave 1242-5 which is fine, but I have been asked about the PPO type for this? how to get this info is that define by the length of the I/o? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/03/2020 13:01:54New subject after splitting |
|
2/3/2020 1:00 PM | |
Joined: 9/27/2006 Last visit: 5/20/2024 Posts: 12257 Rating: (2668) |
Hello sajz; PPO is a term used exclusively for Profibus data exchanges in the Profidrive profile; "PPO" is used when using a ProfiDrive-enabled drive as a Profibus slave (from Siemens, ABB, Danfoss...), to set the data exchange structure between the master and the slave (also known as telegrams). The screenshot below will show you the 5 available PPO structures, from the MicroMaster Profibus Option Board manual. https://support.industry.siemens.com/cs/ww/en/view/6586565 This question about PPO between a Profibus-DP master and a CM 1242-5 as Profibus slave has no application, since Profibus data exchanges between a master and i-slave (intelligent slave) are freely established on configuration, both in the master and the slave. To setup the CM 1242-5 as a slave in the master's configuration, you will need to integrate the gsd )file for the slave module (in the master's Profibus configurator): https://support.industry.siemens.com/cs/it/en/view/49852283 Once that is done, you need to establish the data exchange configuration between master and slave. The following discussion could help point you in the right direction: See the Operating Instructions for CM 1242-5 for more technical details: Hope this helps, |
Last edited by: dchartier at: 02/03/2020 13:01:39 |
|
Follow us on