2/7/2022 2:43 PM | |
Joined: 2/24/2017 Last visit: 2/23/2024 Posts: 3 Rating:
|
Hi, does the edge device have internet access? Because it needs internet access for downloading the needed packages for the nodes. If your edge device have no internet connection, or you want to import the influxdb node offline you need to add the "bundledDependencies" to the package.json file which you downloaded from github. Therefore navigate to the package.json file and add the following bundledDependencies after the existing dependencies: "dependencies": { "influx": "5.6.3", "@influxdata/influxdb-client": "^1.8.0", "lodash": "4.17.21" }, "bundledDependencies": [ "influx", "lodash", "@influxdata/influxdb-client" ] After that run the npm pack again to build the .tgz file and import it again to the FlowCreator. Further information of the bundledDependencies can be found here. |
Last edited by: jhelsper at: 02/07/2022 14:45:29Last edited by: jhelsper at: 02/07/2022 14:59:27 |
|
This contribution was helpful to
1 thankful Users |
Follow us on