9/2/2016 9:51 AM | |
Joined: 11/14/2008 Last visit: 5/6/2024 Posts: 504 Rating: (22) |
Hi, In attachment several print screens. As you can see in print screen starter_1 it's not possible to connect to drive. I do have connection because I can ping PLC (CP-card) and go online in PLC code. AttachmentPGPC_Netpro_Starter.zip (140 Downloads) |
9/2/2016 10:08 AM | |
Joined: 7/22/2008 Last visit: 4/14/2022 Posts: 1884 Rating: (174) |
Is your network card in the same network? Can you ping the device? Is there a virus scan or firewall activ? |
~(‾▿‾)~ |
|
9/2/2016 10:11 AM | |
Joined: 11/14/2008 Last visit: 5/6/2024 Posts: 504 Rating: (22) |
Drive is on Profibus. CP card on IE. And yes I can ping CP. |
9/2/2016 10:21 AM | |
Joined: 11/14/2008 Last visit: 5/6/2024 Posts: 504 Rating: (22) |
No it doesn't find the specific PLC (cp-card) :s |
Follow us on