9/22/2010 9:02 PM | |
Joined: 1/5/2007 Last visit: 4/7/2023 Posts: 1690 Rating: (580)
|
Hi Kolt, sorry LOGO-Barbarian, i have an other opinion about a possible solution of your aim. Plaese look at my answers under "CO2 calculation - Math equations with LOGO!" Best regards Perhaps helpful links: |
==> Meine TAG-Listen: "deut." |
|
This contribution was helpful to1 thankful Users |
9/25/2010 3:23 PM | |
Joined: 1/5/2007 Last visit: 4/7/2023 Posts: 1690 Rating: (580)
|
Hi LOGO!-Barbarian, hi Kolt, At "CO2 calculation - Math equations with LOGO!"i have tell you two concepts to use non-linear fuctions with the LOGO!: a) Approximation of the distributionfunction through one or several with the LOGO! calculable polynomials of 1st to 3rd grades. my Examples: DEMO_Kurveninterpolation (0BA6).zipand FORUM_Kompressor.zip) and specialexample for (nearly) sin-function at Astro Uhr, page 6, file: DEMO_Astro_Uhr_mit Tageseingabe_per_Taster_V3 (0BA6).zip b) Approximation of the distribution function about a table. In the case of clever combination and parameter selection a connection is let between an analog range of values (for example 200..1000) and a value table with n values build up. One needs n - 1 blocks for that then. These are [n - 1] / 3 multiplexer (integer value, round up) and twice so many threshold value switches to their activation. The multiplexers then forms by references a chain, so that the last one outputs the in each case valid value then. my Examples:DEMO_CO2_calculation__Math_equations_with_LOGO (0BA6).zip The sin-funktion is a non linear function and it can aproximated as table of values or as (as example) two linear polynoms and two polynoms with second order (in the ranges of the maximal values of sin-function). Example look at Astro Uhr, page 6, Kolt must define his funktion and go one of the ways i have described...perhapps he can tell us his detailed function [in my opinion T(day time)].... Best regards Perhaps helpful links: |
==> Meine TAG-Listen: "deut." |
|
This contribution was helpful to1 thankful Users |
Follow us on