6/25/2013 2:16 PM | |
Posts: 215 Rating: (6) |
Hello Khoa, first of all: the IP seems to be right because you can download the program. You could also try to ping the PLC to check the link. If you want to see which devices are accessible you have to look up the interface inthe system settings. Please check the entries in "accessible devices" to be equal to the system settings (please refer to the screenshots you find in the ZIP). The moment the entries are right the PLC will be listed. Good luck and best regards AttachmentD:\temp\TIA Portal V12 Error not found devices on the network.zip (396 Downloads) |
Follow us on