4/15/2019 5:52 AM | |
Posts: 2 Rating: (0) |
Why can't TIA Portal detect devices when no windows firewall or anti virus firewall? Always failed to detect the devices..
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 4/15/2019 6:40:46 AMNew subject after splitting |
|
4/15/2019 5:59 AM | |
Posts: 1283 Rating: (105) |
First thing, whether you can ping the device? next are you sure you are using wireless mode of connection to plc? |
4/15/2019 12:57 PM | |
Joined: 7/9/2015 Last visit: 10/15/2024 Posts: 3976 Rating: (592)
|
Hi, reason could be a defect Software Interface but you can reapir it - check the following FAQ: How do you generally parameterize the PG/PC interface and how do you ensure that the device driver can be selected and is visible?If you communicate over Routers / VPN you also should check if all needed ports are unlocked. The most important port ist 102. Regards, Towome |
|
|
Follow us on