11/6/2019 10:55 PM | |
Joined: 11/6/2019 Last visit: 3/13/2022 Posts: 5 Rating:
|
Hi All, A couple of quick questions? We had a TP177A Touch Panel go Down with the LED back light gone. I managed to backup the Touchscreen using WinCC 2008 SP2 to a PSB File. Everything transferred OK. But when I fitted a replacement screen, the Transfer started OK, But failed on File 4 of 4, Transferring the OS. I tried the transfer a few times & it was the same result each time.. I then tried to manually update the OS from within WinCC 2008 SP2 & it again failed.... When I removed the 24v to the panel to see whether a power-cycle would rectify any issue, the Panel is now stuck in a booting-loop, I assume because it has no OS... Is this recoverable? Please see the Movie video attached... https://www.dropbox.com/s/3gluv7o513abk07/IMG_0717.mov?dl=0 The second question is, why did this happen? Both Panels were TP177A's, but the actual SIEMENS Model numbers were different by 1-Digit.... The one with the duff backlight was 6AV6 642-0AA11-0AX1 The bricked one has a model number of 6AV6 642-0AA11-0AX0 Looking on the SIEMENS Website, the one finishing in 1, is a slightly newer model, than the one ending in 0. Does the fact that it failed to load the OS on the older one, mean you can't back up a 1 Model number & restore to a 0 model number? Is it to do with a possible firmware discrepancy of the two models? Any enlightenment to what has happened would be greatly appreciated!!!! Peter |
11/7/2019 2:53 AM | |
Posts: 1 Rating:
|
Hello Friend, Quick Question, Are You Using an MPI Cable as your comms method? |
Follow us on