6/25/2020 10:03 AM | |
Posts: 29 Rating: (0) |
I am using a weekly timer and selecting the days of the week from buttons on the hmi. Is there anyway that the colour can be changed if the button is selected so that the operator sees that the button has been pressed I am using a KTP700 basic panel ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/25/2020 10:40:46New subject after splitting |
|
6/25/2020 3:43 PM | |
Posts: 29 Rating: (0) |
logo plc and tia 15 v1 |
6/25/2020 3:52 PM | |
Joined: 12/18/2014 Last visit: 10/4/2024 Posts: 33876 Rating: (4213) |
And think I right, you need an example? |
6/25/2020 4:01 PM | |
Joined: 12/18/2014 Last visit: 10/4/2024 Posts: 33876 Rating: (4213) |
Siemens created an example years ago with TIA V13 SP1. I upgraded this project to V15.1. Look at the properties of the buttons on the "Animations" tab.
AttachmentWeekly_timer_V15.1.zip (133 Downloads) |
6/29/2020 11:34 AM | |
Posts: 29 Rating: (0) |
attached file
AttachmentSteam Valve control.zip (116 Downloads) |
Follow us on