12/3/2021 7:01 PM | |
Posts: 15 Rating: (0) |
I just received the new Siemens Logo! CIM. It is a cross between the LOGO! CMR and LOGO! CSM. I think it should do all I need it to, if I could get it to work. It has the 4-port switch of the CMS and the Logo! 8 interface plus cellular connection of the LOGO! CMR. It is missing the four digital I/Os of the CMR but has a Modbus RTU interface. I’m not sure about sending emails though, as the documentation does not indicate it will. I have been waiting for seven years for Siemens to release a North American version of the LOGO! CMR. The new CIM comes without the cellular engine, so you can install a cellular engine to work with any region. See Product note Entry ID: 109803292, Entry date: 10/05/2021 I have installed the cellular engine, antennas, and SIM card and all looks good according to the status lights, but I cannot get a computer to connect to the CIM web server. I’m going to start a new post with this question. If we can make it work, I think this will be a great benefit to the North American market and a good option for regions where the CMR will work. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/06/2021 10:14:15New subject after splitting |
|
12/6/2021 10:39 AM | |
Joined: 6/19/2017 Last visit: 5/14/2024 Posts: 8048 Rating: (164) |
Closed cause question posted twice. The second thread with the subject Can't connect to Logo! CIM is published within the conference LOGO! - Communication. Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on