3/22/2006 10:53 AM | |
Posts: 10 Rating: (0) |
Hi, I install a non Siemens CF Card on a MP370 to test the sm@rtservice download files function,but panel don't recognize the card [:(]. Does it exist a generic driver for CF Card? thank you for your help |
3/22/2006 1:33 PM | |
Posts: 3149 Rating: (171)
|
Hi, normally I am using CF cards from sandisk and those cards are working fine [:)] nemo |
3/23/2006 10:14 AM | |
Posts: 10 Rating: (0) |
Hi Nemo, Yes I use a MP370!!! Try another way. I wanna store alarm historical in a CF Card ,and have the possibility to download it using sm@rtservice .Do you know if it's possible? I don't want to buy a CF card without being sure it works... |
3/23/2006 10:40 AM | |
Posts: 3149 Rating: (171)
|
Hi Jule, the following protool faq is valid for WinCC flexible, too: http://support.automation.siemens.com/WW/view/en/5155752 I don´t think that´s possible e.g. to save alarms from panel1on a CF-card in panel2 via sm@rtservice. You will only see the screen of panel1 on panel2, the alarms remain on panel1. nemo |
3/23/2006 11:18 AM | |
Posts: 10 Rating: (0) |
Hi Nemo, I think you won't see waht I wanna do. I explain:I wana store alarm historical in CF Card in a MP370,and have the possibility to download the *.csv file in PC via ethernet using sm@rtservice. I think it's possible but I'm not sure... have an idea? |
3/23/2006 1:40 PM | |
Posts: 3149 Rating: (171)
|
Hi Jule, yes, it´s possible to store your alarms on a CF-Card at panel1 and then access this data via Sm@rtService. You should choose sequential circular logs for your archives => only 1 archive is in "work" and the rest of your archives can be transfered http://support.automation.siemens.com/WW/view/en/22700159 regards, nemo |
Follow us on