6/18/2020 10:00 PM | |
Joined: 12/18/2014 Last visit: 6/9/2024 Posts: 33166 Rating: (4098)
|
Hello Gerard Buist, at first welcome to the forum. Yes, exchange a life bit between the two LOGO!s. |
6/18/2020 10:48 PM | |
Joined: 1/7/2020 Last visit: 5/30/2024 Posts: 9 Rating: (0) |
Like this? |
6/19/2020 4:30 AM | |
Joined: 12/18/2014 Last visit: 6/9/2024 Posts: 33166 Rating: (4098)
|
In attachment there is a little example. Every LOGO! sends a bit to the other LOGO !. Due to an asynchronous pulse generator, this bit is high for 1 second and then low for one second. AttachmentCommunication_monitoring_for_two_LOGO!s_0BA8.Standard.zip (173 Downloads) |
This contribution was helpful to2 thankful Users |
6/19/2020 6:22 PM | |
Joined: 1/7/2020 Last visit: 5/30/2024 Posts: 9 Rating: (0) |
Thanks, working great! |
This contribution was helpful to1 thankful Users |
6/19/2020 6:24 PM | |
Joined: 12/18/2014 Last visit: 6/9/2024 Posts: 33166 Rating: (4098)
|
Hello Gerard Buist, you're welcome ... |
Follow us on