7/22/2022 11:57 AM | |
Joined: 4/28/2015 Last visit: 4/11/2024 Posts: 2 Rating: (0) |
I have a PXC00-E96.A to communicate a 3rd party power meter through TCP/IP. It have 10 devices at IP gateways ( slave address form 11 to 20). And the problem is the initial 3 device always no response(). But using the modbus poll software can get the data from the failed device. Is this the controller problem, or others error? AttachmentDisgonstic capture.xlsx (550 Downloads) |
Follow us on