3/26/2020 7:10 AM | |
Posts: 174 Rating: (2) |
tp1500 comfort v2 |
3/26/2020 7:36 AM | |
Joined: 9/9/2014 Last visit: 6/3/2024 Posts: 246 Rating: (40) |
Look this FAQ How do you evaluate the "RUN / STOP" mode of the CPU via an HMI operator panel? then use this information to overwrite the value in the input / output fiel... For example, using a script, or using a script and scheduler task OR use this: How can you visualize the current status of the CPU on a WinCC flexible operator panel? there is already more information (example for the 300 series) |
Last edited by: Unreality at: 03/26/2020 07:39:11Last edited by: Unreality at: 03/26/2020 07:39:26Best Regards |
|
3/26/2020 9:35 AM | |
Posts: 174 Rating: (2) |
I understood life bit concept for PLC stop. Is there any option to make HMI IO field #### when PLC go into STOP? When PLC go to STOP, HMI showing last good value. |
Follow us on