7/30/2013 2:20 PM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hi Look this thread: Scaling Question |
7/31/2013 5:22 PM | |
Posts: 3 Rating: (0) |
Attached is a simple readout that I'm looking for, but it won't compile because I have no outputs attached. I could also do with know if it's correct what I've put in to read 0-600c. I'm assuming when I run the simulation that I've put the slider up to 600c that it's equivalent to a 10v input on the analog contact? You might have to change the file extension back to .rar Basically I could do with looking at an example if anyone has one. Thanks in advance AttachmentTest K type.zip (240 Downloads) |
Last edited by: The Beginner at: 7/31/2013 5:27 PMLast edited by: The Beginner at: 7/31/2013 5:25 PM |
|
Follow us on