11/20/2023 12:24 PM | |
Joined: 5/6/2022 Last visit: 4/30/2024 Posts: 414 Rating: (82) |
HiTyhoon, In this case, if the screen has a license loaded, before updating the image you must make a backup of the license from the ALM so as not to lose it. Here is how to do it: Because in the end, if there is a license and you do a restore, you will lose it. If you lost it, you would have to contact support to recover the license in which they will ask you for the certificate. Best regards!
|
If this Information really helps, you could use the Rate function |
|
11/21/2023 1:40 AM | |
Joined: 9/1/2010 Last visit: 4/30/2024 Posts: 27 Rating: (0) |
Thanks for the feedback, looks simple enough, however there is no options for KTP600 Basic only 400 and 700? |
Follow us on