4/4/2019 2:06 AM | |
Joined: 9/27/2006 Last visit: 8/11/2024 Posts: 12275 Rating:
|
Hello oleksandr; To understand the complete order code for an instrument, you have to study the catalog for that family of sensors. Especilly this extract: ■Integration The complete flowmeter consists of a flow sensor and an associated transmitter SITRANS F M MAG 5000, MAG 6000 or MAG 6000 I. The flexible communication concept USM II simplifies integration and update to a variety of fieldbus systems, e.g. HART, DeviceNet, PROFIBUS DP and PA, FOUNDATION Fieldbus H1 or Modbus RTU/RS 485. Catalog sheet SITRANS F M MAG 5100 W https://support.industry.siemens.com/cs/ww/en/view/109764956 Look on page 3/96 for the explanation of the order code you provided.7ME6520-3MC13-2KA1 7ME6520 Sensor SITRANS FM MAG 5100 W 4P Diameter DN200 (8”) B Flange Pressure rating PN10 1 Flange material Carbon Steel 3 Sensor liner NBR hard rubber 2K Transmitter MAG 5000, AC power A NO FIELDBUS COMMUNICATIONS PROVIDED 1 Cable Gland Polyamid for MAG 5000 At first glance at the table on age 3/94, for your DN and PN values, it would seem that nominal flow would be 630 m3/h, max flow would be 787.5 m3/h. On page 3/98 you will find a separate order code to get the MAD 5000 transmitter with display. Whenever you decide to go through with such a purchase, I strongly recommend you contact your nearest Siemens rep, who will have access to Siemens instrumentation specialists. They will be able to guide and help you in your selection. Thee is nothing as irritating as discovering your purchase does not match your process requirements, and you have to wait another 12 weeks for a replacement. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 4/4/2019 2:13:26 AMLast edited by: dchartier at: 4/4/2019 2:16:36 AM |
|
4/5/2019 11:18 PM | |
Joined: 9/27/2006 Last visit: 8/11/2024 Posts: 12275 Rating:
|
Hello oleksandr; Unfortunately, answering your question is not as easy as you seem to think. Instrumentation and process control is a very different world that digital programming, and before you start asking us to provide the answers you must first understand what you are discussing. I would respectfully ask you to start with a small document explaining the physics of flowmeters, especially chapter 3: Metrological requirements: http://www2.danak.dk/metrologi/pdf/R49-1.pdf In it you will find the definition (in section 2.3, Operating condirtions)and use of parameters Q1,Q2, Q3 and Q4 in the selection of the flowmeter model (in section 3) that are used in the tables and graphics you showed earlier for the Siemens FI01 catalog. You will probably be able to answer your own questions better then. Next, before the final selection of the instrument, information on these different values of flow in your process must be provided by a competent process engineer, usually in the form of a PFD (process flow diagram). This will give you the exact ranges of flow and pressure measurement and turn-down that the flowmeter must be able to withstand and measure correctly. Hope this helps, |
Last edited by: dchartier at: 4/5/2019 11:31:21 PM |
|
5/15/2020 12:06 PM | |
Joined: 3/28/2010 Last visit: 8/5/2024 Posts: 1051 Rating:
|
In answer to what I think are your questions: The flow tube, the part that goes in the piping, determines the maximum flow rate, not the electronic 'transmitter/converter box. The flow rate ranges depend on the magtube's size/diameter. AttachmentSizing tables from 5100W manual Nov 2010.pdf (354 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on