8/8/2014 11:17 AM | |
Posts: 1368 Rating: (126) |
hello, i do not know PH controller and D.O. controller, so...only an idea: Can you use OPC? |
8/8/2014 1:51 PM | |
Joined: 10/28/2008 Last visit: 7/21/2023 Posts: 245 Rating: (14) |
Hi. Whats the distances and which interfaces are available on your equipments ?
|
Georgio |
|
8/21/2014 8:29 AM | |
Posts: 80 Rating: (1) |
4-20 mA outputs are available from the devices? The problem is how do I select the RD500 and which I/O modules shall I order with it?
|
8/21/2014 5:33 PM | |
Joined: 12/16/2010 Last visit: 5/1/2024 Posts: 9 Rating: (2) |
The RD500 is ideal for this application. You can monitor real time via MODBUS TCP or collect the datalogs via FTP or Email. The RD500 will allow a view of the process via the onboard Web sever. See attached part numbers for the RD500 and modules. The RD500 includes a 1GB CF card for datalogging. AttachmentD:\tmp\upload\RD500.pdf (122 Downloads) |
Last edited by: CS Moderator at: 8/29/2014 9:09 AMAttachment reattached |
|
This contribution was helpful to1 thankful Users |
Follow us on