3/10/2009 2:31 PM | |
Posts: 3 Rating:
|
Sorry, I hadn't specified that the error regard the FB66 T_DISCON |
3/25/2009 1:58 AM | |
Posts: 27 Rating:
|
WinAC can communicate with other pc using T-block functions via Open IE. three keypoints are: 1.NIC should be Intel Pro/1000PL(chipset:I82573). 2.based on which IFused byNIC, DEV_ID is: IF1: DEV_ID = B#16#01 IF2: DEV_ID = B#16#06 IF3: DEV_ID = B#16#0B IF4: DEV_ID = B#16#0F 3.software requirements(my testing envirenment): step7 5.4 sp4, HSP 2009-2 WinAC RTX 2008 sp1 and you can download the sample from the following link, then change DEV_ID according to your configuration: http://support.automation.siemens.com/WW/view/en/29737950 Sample_open_TCP.zip Good Luck! |
This contribution was helpful to
2 thankful Users |
3/26/2009 1:14 PM | |
Posts: 3 Rating:
|
Very good... in the open IE standard block manual wasn't written that the DEVICE ID is different for the WinAC processor... Thanks so much |
4/27/2009 1:05 PM | |
Posts: 89 Rating:
|
but it is written in the WinAC manual |
Follow us on