2/9/2019 10:19 PM | |
Joined: 11/15/2017 Last visit: 9/2/2022 Posts: 87 Rating: (0) |
Hello, Just a quick question I have attached a code(Mitsubishi) I would like to to re-write using the logo 1. is it feasible 2.what would be the pitfalls regarding migration of the code,because I am not to familiar with Mitsubishi.Hope some could point me in the right direction regards Ade Attachmentfx1n_program_para.zip (197 Downloads) |
2/12/2019 11:38 AM | |
Joined: 12/18/2014 Last visit: 6/17/2024 Posts: 33204 Rating: (4107)
|
Then create a program print as a PDF file and upload the print to the forum. |
2/12/2019 1:34 PM | |
Joined: 11/15/2017 Last visit: 9/2/2022 Posts: 87 Rating: (0) |
Here is the the code in pdf format.
AttachmentGX_Developer_print_Ladder_MAIN.pdf (184 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on