12/13/2023 3:26 AM | |
Joined: 12/25/2016 Last visit: 6/1/2024 Posts: 90 Rating: (0) |
What is the use of having memory card in S7-1500? Does it store the program of the CPU? |
12/13/2023 5:46 AM | |
Joined: 1/21/2013 Last visit: 6/8/2024 Posts: 2861 Rating: (458) |
Hi hyo_eddie, The S7-1500 PLCs use the SIMATIC memory card as load memory, which contains code blocks, data blocks, technology objects and the hardware configuration. Since the CPUs have no other way to store this data, the SIMATIC memory card is mandatory. This is slightly different from the S7-1200 PLCs, which have a small internal load memory. Kind regards |
12/13/2023 9:12 AM | |
Joined: 3/11/2019 Last visit: 6/7/2024 Posts: 1460 Rating: (263) |
Hi, in addition to the project, the SMC can hold also other data.
In general this topic is described in the different manuals for TIA or/and S7-1200/1500. Some usecases for example: What you need to know about SIMATIC memory cards regards sancruz |
Feedback appreciated, please rate |
|
This contribution was helpful to2 thankful Users |
Follow us on