3/24/2021 10:23 AM | |
Joined: 12/18/2014 Last visit: 7/31/2024 Posts: 33441 Rating: (4153)
|
Sales and delivery release for firmware V2.1.8 for LOGO! CMR2020 (6GK7142-7BX00-0AX0) and LOGO! CMR2040 (6GK7142-7EX00-0AX0) including downloadThe new firmware V2.1.8 for the LOGO! CMR2020 and LOGO! CMR2040 modules has been released and is now available for download free of charge. The modules are scheduled for delivery starting in 03/2021 with the new V2.1.8 firmware. 1. Product description Firmware version V2.1.8 is the successor of version V2.1.7 and contains function extensions for support of LOGO! CMR communication with the new LOGO! BM 8.3. The firmware also includes general improvements and optimizations. The update to V2.1.8 is necessary for all customers who are using a LOGO! CMR and want to use it to monitor and control a LOGO! BM with the new version 8.3. Due to a security-related change in LOGO! BM 8.3, only an encrypted connection can be used between LOGO! CMR and LOGO! BM as of this version to exchange the process data. This is supported with FW V2.1.8 of the LOGO! CMR. Please observe the notes on parallel access from the LOGO! CMR and LSC/LWE to a LOGO! BM 8.3 and on using the newly introduced SMS commands in the updated manual. The following improvements and optimizations are also being released with firmware V2.1.8:
|
Last edited by: Jen_Moderator at: 03/30/2021 07:34:35Optimized links. Last edited by: Jen_Moderator at: 03/30/2021 07:35:43*missed one part. |
|
Follow us on