5/22/2023 12:48 PM | |
Joined: 5/16/2023 Last visit: 3/19/2024 Posts: 3 Rating: (0) |
Hello, I have a problem with some SD cards 2GB 6av2181-8xp00-0ax0. I use them for system backup in different panels (usually KTP400 or TP1200) and sometimes the system don't want to recognize the card as "Siemens" and ask for replacements. the only difference I noticed is the FS number, that ones with 03 work fine but the ones with 04 or 05 not, and the date and serial number but I don't think that is so relevant. Any idea? Thanks.
AttachmentSD Card.pdf (356 Downloads) |
5/22/2023 1:35 PM | |
Joined: 5/28/2008 Last visit: 5/11/2024 Posts: 4506 Rating: (836) |
Hello, Check if somebody formatted the SD card. If yes, then it is now useless Please see if this will help you: Why is the SIMATIC HMI SD Memory Card not recognized in a Comfort panel? |
Ayman Elotaify |
|
5/23/2023 4:13 AM | |
Joined: 5/16/2023 Last visit: 3/19/2024 Posts: 3 Rating: (0) |
Thx for answer. The cards are new, taked from sealed, original package |
Follow us on