3/24/2021 6:26 PM | |
Joined: 3/24/2021 Last visit: 5/3/2022 Posts: 5 Rating: (1) |
Sorry to mess up this topic. I have troubles too. I can see the Logo! in the pc-to-logo screen and when i try to "Test" the connection it takes a while to come back with an error. I have 2 Logo's on a network, and one is okay to up and download, the other is visible but cannot connect. Tried to reset to factory and connect is directly to PC but no connection is possible. What could be the problem? Could it be that there is a faulty link in my network program that messed up the Logo! ? When i reset the Logo! all should be fine??? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/25/2021 09:09:25New subject after splitting |
|
3/24/2021 6:51 PM | |
Joined: 12/18/2014 Last visit: 8/7/2024 Posts: 33499 Rating: (4162)
|
That is the problem. You have the new LOGO!8.3. For this LOGO! you need LSC V8.3. You can download the upgrade to LSC V8.3 from here: Download for LOGO! 8.3 Software UpgradeBut this download is export restricted and you need a special registration. Why do you have to log in and register for downloading export-restricted software and what data do you need for this? |
This contribution was helpful to1 thankful Users |
Follow us on