7/3/2023 8:22 AM | |
Joined: 5/12/2006 Last visit: 8/14/2024 Posts: 22343 Rating:
|
you must install WinCC Runtime and then start the rt loader on the tablet to download the project from the laptop |
7/3/2023 8:33 AM | |
Joined: 6/30/2023 Last visit: 2/8/2024 Posts: 18 Rating:
|
but how to enable it now? how to start |
7/3/2023 8:40 AM | |
Joined: 5/12/2006 Last visit: 8/14/2024 Posts: 22343 Rating:
|
which wincc exactgly is installed? please give more information about the setup. |
7/4/2023 10:22 AM | |
Joined: 6/30/2023 Last visit: 2/8/2024 Posts: 18 Rating:
|
Simatic_WinCC_Unfiled_PC_V17 |
7/4/2023 11:39 AM | |
Joined: 1/21/2013 Last visit: 8/15/2024 Posts: 3044 Rating:
|
Hi WiktorRoz, You should be aware that the more detailed the description of the problem and the initial situation, the easier it will be to answer the questions. Queries cost time and sometimes nerves. Your screenshot and your last answer show me that you have already installed WinCC Unified PC Runtime V17 on the SIMATIC ITP1000. So one step is already done. Now you need the engineering software. Do you have WinCC Unified V17 installed on your computer? It would also be possible to install this on the ITP1000, but your computer will probably have the better performance. Please note that if you have not yet installed or purchased the software, you may not have a valid license. You can use a trial license for 21 days, but in the case of WinCC Unified PC, the trial license may not cover your needs. Please also note the requirements for the installation of WinCC Unified. When the engineering software is running, you can connect the ITP1000 to your PC via LAN and download the HMI Runtime project to the ITP1000. Alternatively, you can transfer the project using an external storage medium. I hope this explanation will help you in your work. If you have any problems, please let us know. Kind regards |
Follow us on