10/1/2015 12:39 PM | |
Posts: 116 Rating: (2) |
Hi, I work with TP1200. It's just simply stuck with file not exist. I copy pdf file to SD card and configure pdf view as in attached. any suggestion ? ------------------------------------------------------------------------------------------ AttachmentPdf View.zip (312 Downloads) |
Last edited by: Min_Moderator at: 10/1/2015 1:53:19 PMNew subject after splitting |
|
10/2/2015 8:30 AM | |
Joined: 8/3/2009 Last visit: 9/18/2024 Posts: 13728 Rating: (1728) |
Hello Tikki Use as Path \StorageCard USB\yourfilename.pdf you have to set the real Path on the Panel so it is better to test it on the Panel. you can simulateit but sou have to copy the pdf file in the folder "Storage Card USB" in your C Partition on Computer. This folder is simulated by the Engineering System. Bye Murof |
If this Information really helps, you could use the Rate function |
|
3/9/2017 10:45 AM | |
Joined: 1/14/2016 Last visit: 9/13/2024 Posts: 2 Rating: (0) |
Hi Murof, you must add space to path: \Storage Card USB\yourfilename.pdf \Storage Card SD\yourfilename.pdf |
12/15/2017 10:33 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by WI Programmer is split to a separate thread with the subject Where is the directory on C drive? . Best regards |
Follow us on