5/16/2023 8:41 AM | |
Joined: 8/3/2009 Last visit: 8/6/2024 Posts: 13461 Rating:
|
Hello x_Paycheck_x Yes the combination with MPI should work. Check if the 19200 settings in your HMI Connection is correct to the used MPI rate you are using in the PLC (default is usually 187500). first transfer without project you have to set the correct address and baudrate on the Panel (LINK) If the project is loaded and started, the configuration out of the project will run on the panel. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on