1/24/2020 11:46 AM | |
Joined: 11/8/2016 Last visit: 7/23/2024 Posts: 64 Rating: (9) |
Hello BCE, I assume your VPN problem is that your mobile address isn't public. Your IP starts with 10. .. These are normally non-public IP addresses. Therefore you can't connect to it. Which provider / apn do you use? Make sure it is used for public IP addresses. Regarding your mail issue which you fixed. At Gmail you need to allow unsecure apps, as google is acting really "secure" at this kind of things. Regarding the certificate you can load into the CMR. It works without, as the CMR is just using the loaded CMR and compares it with the server ones. If none is loaded, every Server certificate is OK. You can check e.g here https://de.ssl-tools.net/mailservers/gmail.com what certificates google is using and load it into the CMR. This way, you make sure no other server can act like the Gmail.com email server (man in the middle attack |
Follow us on