9/21/2023 7:27 PM | |
Joined: 5/17/2022 Last visit: 7/8/2024 Posts: 1 Rating:
|
Any solution? I get the same warning when I try to upgrade a KTP1000 Basic to a TP1200 Comfort. ------------------------------------------------------------------------------------------ |
Last edited by: Leonel97 at: 09/21/2023 19:28:19Last edited by: Jen_Moderator at: 09/22/2023 09:26:21New subject after splitting |
|
9/22/2023 11:17 AM | |
Joined: 5/30/2022 Last visit: 8/5/2024 Posts: 558 Rating:
|
Hi Leonel97, The messages displayed are simply warnings, you have to manually evaluate the correct operation of all functions. What is TCPKEEPALIVE? Is it a life bit? If it is a life bit, you can use the GETPLCMODE function, here is some information about it: How do you evaluate the "RUN / STOP" mode of the CPU via an HMI operator panel? |
If this information really helps, you could use the Rate function. |
|
Follow us on